AXIS#.VL.KP

Description

AXIS#.VL.KP sets the proportional gain of the velocity loop.

The idealized velocity loop bandwidthClosed In computer networking, bandwidth often refers to a data rate measured in bits/s, for example, network throughput. The reason for the connection of data rate with the term bandwidth is that the limit to the data rate of a physical communication link is related to its bandwidth in hertz in Hz is:

Rotary motor:

BandwidthClosed In computer networking, bandwidth often refers to a data rate measured in bits/s, for example, network throughput. The reason for the connection of data rate with the term bandwidth is that the limit to the data rate of a physical communication link is related to its bandwidth in hertz (Hz) = AXIS#.VL.KP *Kt/ (2π *Jm)

Where:

Kt= motor torqueClosed Torque is the tendency of a force to rotate an object about an axis. Just as a force is a push or a pull, a torque can be thought of as a twist constant, in units of Nm/Arms

Jm = motor inertia, in units of kg*m²

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type

Read/Write

Units

A/(rad/sec)

Range

0 to 2,147,483.008

Default Value

0

Data Type

Float

Stored in Non-Volatile Memory

Yes

Variants Supported

All variants are supported.

Fieldbus Information

EtherCATClosed ***EtherCAT is an open, high-performance Ethernet-based fieldbus system. The development goal of EtherCAT was to apply Ethernet to automation applications which require short data update times (also called cycle times) with low communication jitter (for synchronization purposes) and low hardware costs CoE and CANopen

Command

Index

SubIndex

Data Type

Units

Float Scale

Access

PDOClosed PDO is a type of protocol frame used in some fieldbuses. A PDO contains one or more object dictionary entries, which define the application data transferred between devices. Mappable

AXIS1.VL.KP

5011h

01h

Signed32

-

1000:1

Read/Write

No

AXIS2.VL.KP

5111h

01h

Signed32

-

1000:1

Read/Write

No

EtherNet/IP

Name

ID

Hex

Data Type

Access

Units

AXIS1.VL.KP

6029

178D

Signed32

Read/Write

-

AXIS2.VL.KP

71565

1178

Signed32

Read/Write

-

PROFINET

Parameter

PNU

Data Type

Access

Units

AXIS#.VL.KP

6029

Float

Read/Write

-